{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Updating the version of OFS installed by Vijeo Citect requests a part number and serial number.
Issue
Updating the version of OFS installed by Vijeo Citect requests a part number and serial number.

Product Line
OFS

Environment

Vijeo Ciitect

Resolution
If you try to update the OFS software that is installed as part of the Vijeo Citect installation, the update software will
return a pop-up window requesting a part number and serial number.

The reason this occurs is because the update for OFS is a separate stand alone installation which requires a part number and
serial number to install.  The only method available for updating the OFS software installed by Vijeo Citect is to update the
Vijeo Citect software.