Issue:
Is CANOpen available for the ATV340?
Product Line:
ATV340
Environment:
All non-Ethernet models
Cause:
Wiring
Resolution:
CANOpen is not a standard embedded protocol on ATV340 drives. Obtain a CANOpen option module based on the connection type: VW3A3608 for RJ45
VW3A3618 for SubD9
VW3A3628 for Open style terminal
See attachment.
Note that the ATV340....E Ethernet models will not accept any comms module.
Released for:Schneider Electric Global