{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where can the Digital inputs status be monitored on the Altivar Process Drives?

Article available in these languages: Spanish

Issue:
Need to confirm that the Altivar Process drive is recognizing the digital inputs.

Product line:
ATV600, ATV900, Altivar Process

Environment:
n/a

Cause:
Troubleshooting drive

Resolution:
Push the Home button to get to the Main Menu.
From the Main Menu, navigate to Display -> I/O Map -> Digital Input Map.

It will now display the status of the STOA, STOB and Digital Inputs 1 thru 8.  The contact is closed if the Input shows High (or up).  The contact is open if the input shows Low (or down).

Note:  From this menu, highlight and enter each input to check which functions are assigned to it.