{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to monitor status of Extension card digital and analog signals via web server on Altivar ATV630, ATV930, ATV340...E?
Yes, it is possible. After login to the web server, in the section displaying - I/O status all the inputs are visible. See printscreen.
Analog signals, can be monitored also in the dashboard menu. To be able to see them in the dashboard, it is necessary to create a new table with required variables. See the print screen with added AI4 and AI5 analog signals. Then the table can be added to dashboard as a widget.

Schneider Electric Global

Attachment(s)
WEb_Server_ATV630_IOstatus.jpg [401.95 KB]
WEb_Server_ATV630_Create new table.jpg [167.55 KB]
WEb_Server_ATV630_Add table to dashboard.jpg [359.97 KB]