Issue:
ATV630 speed control with local HMI
Product Line:
Altivar ATV600 and ATV900 series drives
Environment:
All
Cause:
The drive's speed is to be controlled by the local HMI
Resolution:
Enter the Main Menu of the Drive. Go to Complete Settings then go to Command and Reference. In this Menu, the first parameter is Ref Freq 1 Config which is set to AI1 (Factory default), change this parameter to Ref Freq-Rmt Ter
Main Menu -> Complete Settings -> Command and Reference
-> HMI CMD to Bumpless (Default is Disabled)
-> Ref Freq 1 Config -> Ref Freq-Rmt Term
-> If Start/Stop from Terminals and Speed control from HMI, Control Mode must be changed to Separate
ATV630 speed control with local HMI
Product Line:
Altivar ATV600 and ATV900 series drives
Environment:
All
Cause:
The drive's speed is to be controlled by the local HMI
Resolution:
Enter the Main Menu of the Drive. Go to Complete Settings then go to Command and Reference. In this Menu, the first parameter is Ref Freq 1 Config which is set to AI1 (Factory default), change this parameter to Ref Freq-Rmt Ter
Main Menu -> Complete Settings -> Command and Reference
-> HMI CMD to Bumpless (Default is Disabled)
-> Ref Freq 1 Config -> Ref Freq-Rmt Term
-> If Start/Stop from Terminals and Speed control from HMI, Control Mode must be changed to Separate
Released for:Schneider Electric Global