{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Where can I find the Skip frequency parameter settings in the ATV630 process drive?
Issue:
Programming and understand skip frequency function of ATV630

Product Line:
ATV600

Environment:
All serial numbers

Cause:
Prevent prolonged operation within an adjustable range. Minimize noise at (x) frequency.

Resolution:


Jump frequency parameters can be located in  Main Menu  [Complete settings]  -> [Generic Functions] -> [Jump frequency]
3 possible skip frequencies can be added at a time.
Skip frequency hysteresis is the frequency value range skipped.
For example, we have skip frequency value at 30 hz with hysteresis of 3hz.  This means that the frequency range 27-33 will be skipped on ramp.

Schneider Electric Global