{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause an brF or brake feedback fault on the ATV630 or ATV930 drives?
Issue:
ATV630 and ATV930 showing brF or brake feedback fault.

Product Line:
ATV630 or ATV930 drives

Environment:
All

Cause:
The monitoring of the brake (assign the braking contact to a logic input) does not
match the braking command.

Resolution:
brake feedback and the control circuit.
• Check the mechanical state of the brake.
• Check parameter BCI → brake contact input
• Check parameter BLC → brake assignment.
• Check parameter BRT → brake release time.
• Check parameter BET → brake engage time.

Schneider Electric Global