{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause an INF2 or internal error 2 on the ATV630 and ATV930 Process drives?

Issue:
INF2 or internal error 2 on the ATV630 and ATV930 Process drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
The Power board was exchanged by a spare part, and is not configurable to the correct power rating.

Resolution:
Unknown or Incompatible Power Board
Principle

Probable causes:
• The Power board was exchanged by a spare part, and is not configurable to the correct power rating.
Remedies
• Switch OFF/ON the inverter.
• Check the reference number of the power board.
• connect to the SoMove service section and use the "drive type recovery function" to set a valid configuration of the power board.
• Replace the control block

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Global

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: