Issue:
Can SoMove Software be used to monitor multiple drives over a Modbus network?
Product Line:
Altivar Process Drive
Environment:
All models and serial numbers
Cause:
Wiring / Programming
Resolution:
You can use the resident Modbus RTU on the drive so no Gateway is required. You would configure each drive with a Modbus Network address. Cable used to daisychain (VW3A8306TF03 or ..F10) via Modbus.
The cable is F03=.3 M or 1ft, or 10= 1.0M or 3ft. Set the Scan up as Multipoint, and have to setup the range of registers.
Can SoMove Software be used to monitor multiple drives over a Modbus network?
Product Line:
Altivar Process Drive
Environment:
All models and serial numbers
Cause:
Wiring / Programming
Resolution:
You can use the resident Modbus RTU on the drive so no Gateway is required. You would configure each drive with a Modbus Network address. Cable used to daisychain (VW3A8306TF03 or ..F10) via Modbus.
The cable is F03=.3 M or 1ft, or 10= 1.0M or 3ft. Set the Scan up as Multipoint, and have to setup the range of registers.
Released for:Schneider Electric Global