Search FAQs
How is the ATV340 drive programmed to start stop from terminals and use HMI for speed control?
Issue:
Programming an ATV340 to use the dial of HMI for speed reference and digital input (DI1) for Start/Stop controlProduct Line:
Altivar 340, ATV340
Environment:
All
Cause:
Programming setup
Resolution:
In the Main Menu, select Complete Settings, then Command and Reference.
Set [Ref Freq 1 Config] Fr1 to [Ref Freq-Rmt Term] LCC
Set [Control Mode] CHCF = [Separate] SEP
Verify [Cmd channel 1] CD1 = [Terminals] TER
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: