{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the Windows 10 full version version recommended on the Magelis HMIBMU Modular Box PC Universal?
Issue
Is the Windows 10 full version version recommended on the Magelis HMIBMU Modular Box PC Universal?

Product Line
Magelis Modular Box PC HMIBM Universal (HMIBMUHI29D2801, HMIBMUSI29D2801, HMIBMUCI29D2W01, HMIBMU0I29D2001, HMIBMU0I29D200A, HMIBMUHI29D4801, HMIBMUSI29D4801, HMIBMUCI29D4W01, HMIBMU0I29D4001, HMIBMU0I29D400A, HMIBMU0I29DI00A, HMIBMU0I29DE00A)

Resolution
The Magelis HMIBMU Modular Box PC Universal iPC Magelis has a 1.6GHz Celeron 2980U, which is only a Dual Core CPU with 8GB DD3 RAM meant for ultra-low power consumption applications.
Even though the full Windows 10 minimum requirements are a 1.0 GHz Dual-core CPU with 2GB RAM, a more realistic requirement would be for a Quad Core 2.0GHz with minimum 4GB of RAM.

The HMIBMU is sold with Windows 10 IoT Enterprise Edition (which is a smaller and less demanding version of Windows 10). This would be the version of Windows 10 recommended for install for the best performance.

Schneider Electric Global