{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where do I find the Magelis HMIG5U2 OS Image?

Issue

Where do I find the Magelis HMIG5U2 (Windows Embedded Standard) OS Image?

Product Line

Magelis HMIGTU Series

Resolution

The Magelis HMIG5U2 OS Image can be found attached to this FAQ:


HMIG5U2 BIN Image file (7.3GB): HMIG5U2_V400_20190227.bin
-> This is attached as 8 separate 7-zip files ("HMIG5U2_V400_20190227.7z.001" through to "HMIG5U2_V400_20190227.7z.008"). You will need the 7-zip extraction tool from www.7-zip.org to extract the .BIN file.


Backup Recovery Tool v1.0.4.2 (3MB): BackupRecovery.exe
MD5 Hash (of the .exe): db3b62d9428c07decd06680cd4fada36
-> This is attached as "BackupRecovery_v1.0.4.2.zip" (a regular zip file that you can doubleclick on to open in Windows to extract it)


How to extract the .BIN file from the eight 7z files:
All the files are downloaded into the C:\HMIG5U2_v400\ folder here.
Open the folder in 7-zip, then double-click the HMIG5U2_V400_20190227.7z.001 file (green arrow):
Using 7-zip application to extract the archive from multiple files
That will reveal the .BIN file, where you can drag and drop it into a folder of your choice:.bin file is revealed in 7-zip; drag and drop to a folder in Windows Explorer


Note: This .BIN image file is not the same as for the older generation HMIG5U.

Schneider Electric Global

Attachment(s)
HMIG5U2_V400_20190227.7z.001 [1000 MB]
HMIG5U2_V400_20190227.7z.002 [1000 MB]
HMIG5U2_V400_20190227.7z.003 [1000 MB]
HMIG5U2_V400_20190227.7z.004 [1000 MB]
HMIG5U2_V400_20190227.7z.005 [1000 MB]
HMIG5U2_V400_20190227.7z.008 [292.96 MB]
HMIG5U2_V400_20190227.7z.006 [1000 MB]
HMIG5U2_V400_20190227.7z.007 [1000 MB]
BackupRecovery_v1.0.4.2.zip [1.35 MB]