{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the replacement part number for the MCB or Main Control Board for the ATV930 or ATV960 Drives?
Issue:
Part number for Main Control Board for ATV930/ATV960

Product Line:
ATV930 and ATV960 Drives

Environment:
All

Resolution:
The MCB or Main Control Board pat number for the ATV930, ATV980 or ATV960 drive is VX4B900100.
Note: This part can be ordered, however, be aware that this is not a standard part.
**For use in High HP ATV960 or ATV980 a change, that can only be made by Schneider Electric Services, may be required.
Contact Drives Technical Support at 888-SquareD or 888-778-2733.