Issue:
ATV630 and ATV930 drive for damper control.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Damper control option
Resolution:
Damper Control in Altivar Process ATV630
The Altivar Process 600 drives were not designed specifically for HVAC applications in the way
the Altivar 212 drives were, and do not include dedicated ‘Damper Control’ functions. You can,
however, use the ‘Priming Pump’ control function to control a damper in a similar way.
Use ‘Priming Pump Assignment’ (PPoA) to select the output relay to send the open/close
command.
Use ‘Primed Switch Assign’ (PPWA) to set the logic input for the damper position feedback
input.
Use ‘Priming Time’ (PPSd) to set the delay time from sending a damper open command to the
drive starting the fan rotation.
This does not provide quite the same level of interlocks and error detection that is in the
ATV212 functions, but does allow basic damper control within the drive.
This does not apply to the ATV930 drive which does not have any options for Damper control.
ATV630 and ATV930 drive for damper control.
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Damper control option
Resolution:
Damper Control in Altivar Process ATV630
The Altivar Process 600 drives were not designed specifically for HVAC applications in the way
the Altivar 212 drives were, and do not include dedicated ‘Damper Control’ functions. You can,
however, use the ‘Priming Pump’ control function to control a damper in a similar way.
Use ‘Priming Pump Assignment’ (PPoA) to select the output relay to send the open/close
command.
Use ‘Primed Switch Assign’ (PPWA) to set the logic input for the damper position feedback
input.
Use ‘Priming Time’ (PPSd) to set the delay time from sending a damper open command to the
drive starting the fan rotation.
This does not provide quite the same level of interlocks and error detection that is in the
ATV212 functions, but does allow basic damper control within the drive.
This does not apply to the ATV930 drive which does not have any options for Damper control.
Released for:Schneider Electric Global