Issue:
Can the ATV630 drive be configured to maintain a constant pressure, using the Sensorless flow estimation function?
Product Line:
ATV630
Environment:
All serial numbers
Cause:
No external PI control
Resolution:
No, it is not possible to maintain constant pressure control with Sensorless Flow Estimation.
Can the ATV630 drive be configured to maintain a constant pressure, using the Sensorless flow estimation function?
Product Line:
ATV630
Environment:
All serial numbers
Cause:
No external PI control
Resolution:
No, it is not possible to maintain constant pressure control with Sensorless Flow Estimation.
Released for:Schneider Electric Global