{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the basic keypad VW3A1113 on Altivar340 variable speed drive be used for switching from HMI control to remote?
Basic keypad VW3A1113 does not have loc/rem button, so it is not possible to switch from local to remote using a single button.
Advanced keypad VW3A1111 has loc/remote button, so it is one of the solution.
With basic keypad you can only do change from local to remote and opposite by entering 5.3 command and reference menu and change frequency reference (FR1) parameter.

Schneider Electric Global