Is there a Magelis HMI series that is rated for outdoors?
Published date:
08 March 2019
Is there a Magelis HMI series that is rated for outdoors?
Magelis HMIGTUx series
The Magelis HMIGTUx series (HMIG3x with HMIDT35x, HMIDT65x, HMIDT75x) is rated for outdoor use. The screen is rated at 1000 cd/m2 and is suitable for bright outdoor applications. The range of temperatures that the units can be used in are as follows:
HMIDT35x: -30...65 °C (-22...149 °F)
HMIDT65x: -30...70 °C (-22...158 °F)
HMIDT75x: -20...60 °C (-4...140 °F)
The HMIGTUx series is supported by Vijeo Designer V6.2 SP8