{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Ethernet IP Add-On-Profile for Altivar Process drives
Issue:
Is there an Add-on Profile available for Altivar Process Drives and Ethernet IP?

Product Line:
ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
There is no dedicated Add-On Profile (AOP) available for the Altivar Process series drives.
We only provide the EDS file to integrate the drive inside Rockwell PLCs.

Schneider Electric Global