{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I get a second analog output on the ATV340 drive?
Issue:
Is it possible to add a 2nd analog output on the ATV340 Drive?

Product Line:
ATV340

Environment:
All

Cause:
Customer needs a second analog output. Looking for an I/O expansion module

Resolution:
No. There are only 2 I/O expansion modules for the ATV340 drive. The VW3A3203 has 6 digital inputs, 2 digital outputs, and 2 analog inputs, and the VW3A3204 has 3 relay outputs.

Schneider Electric Global