Can an Ethernet module be added to a "Non-E" version of an ATV340 series drive?
Published date:
22 May 2019
Issue:
Customer has purchased a "non-E" version of the ATV340 drive but needs to communicate with the drive via Ethernet.
Product Line:
ATV340 series drives
Environment:
"Non-E" version of the drive (last digit of part number is NOT an E)
Cause:
Clarification of product capabilities.
Resolution:
No. An ATV340 drive that does not have integrate Ethernet communication options can not have them added via an option card. There are two versions of the ATV340 series drive, the E and the Non-E. If Ethernet communication is needed you must purchase the E version (Last digit of part number is E).
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.