{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the default Windows password for the HMIG5U/HMIG5U2?
Issue:
The default Windows password for the HMIG5U/HMIG5U2 cannot be found in any documentation.

Product Line:
HMIG5U/HMIG5U2

Resolution:
The HMIG5U/HMIG5U2 are setup without a Windows login password by default. If you require one, please create a user and password in the Windows Control panel under User management. If there is a password setup on your HMIG5U/HMIG5U2 and you do know know what it is, you can always restore the CFast card back to factory OS settings using the recovery DVD that comes with the HMIG5U/HMIG5U2.

Schneider Electric Global