{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can I change the relay status from NO to NC on the Altivar Process Drives?
Issue:
They need to change the function of the output relay from Normally Open contact to a Normally Closed contact.

Product line:
Altivar Process, ATV600 ATV900

Environment:
all

Cause:
The Altivar Process drives come with only R1 having a normally open and normally closed contact.  R2, R3 and the extended IO Card relays are all Normally Open only.

Resolution:
Under the Relay configuration menu (i.e. R2 Configuration > go to R2 Active at.  The factory setting is 1 (closed).  Change this value to 0 for active when open to invert the relay output signal.

NOTE:  Operating State Fault (FLT) cannot be assigned to 0.  If an additional NC contact is needed for Fault indication, add an external control relay with the additional contacts.

Schneider Electric Global