{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause an INFG or internal error 16 on the ATV630 and ATV930 drives?
Issue:
What is the internal error 16 or INFG on the ATV630 and ATV930 drives?

Product Line:
Altivar Machines, Altivar Process Drives

Environment:
All model numbers, all serial numbers

Cause:
It can be caused by internal CPU error.

Resolution:
  • Verify that the option module is correctly connected to the slot.
  • Replace the option module.

Schneider Electric Global