Issue
RAM and CPU usage are high, but PME is not logging new data
Product line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Microsoft Windows 10
Cause
"ION Log Subsystem Router Service" runs the stored procedure “RebuildAlarmRelatedIndexes” to rebuild indexes on major ION_DATA tables.
For large databases, it may take longer and affect system performance.
Resolution
Update the stored procedure to do a REORGANIZE vs a REBUILD function on the indexes.
The attached SQL file will make the required changes in the "RebuildAlarmRelatedIndexes" stored procedure.
Released for:Schneider Electric Global