Issue
When the diagram was created in Vista several numeric objects were made. These numeric objects showed up on the WebApps Diagrams page in a blue font different from the black font that was used when they were created in Vista.
Product Line
PME 9.0
PME 2020
Environment
Web Applications - Diagrams
Vista
Cause
This is happening because the Web Diagram will treat the object as a hyper-link. It is treated like a hyperlink because the numeric object has an action associated with it. Showing it as a hyperlink is to show users that it is a click able object with an action associated with it. This is how PME should behave.
Resolution
In the case thatFA386845 does not work here is an alternative fix.
When the diagram was created in Vista several numeric objects were made. These numeric objects showed up on the WebApps Diagrams page in a blue font different from the black font that was used when they were created in Vista.
Product Line
PME 9.0
PME 2020
Environment
Web Applications - Diagrams
Vista
Cause
This is happening because the Web Diagram will treat the object as a hyper-link. It is treated like a hyperlink because the numeric object has an action associated with it. Showing it as a hyperlink is to show users that it is a click able object with an action associated with it. This is how PME should behave.
Resolution
In the case thatFA386845 does not work here is an alternative fix.
- In Vista go to the configuration of the numeric object.
- In the action tab, select None. Press Okay.
- Grab a grouping object from the tool bar and place it over the existing numeric object.
- In the configuration for this object set the Display to None.
- While in the configuration change the action to the desired action (i.e. Open Diagram for Meter Template)
- Press Okay in the Configuration, and then save the file.
- Refresh the WebApps page.
Released for:Schneider Electric Global