{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PME maintenance tasks fail with error 0x1F4 if IONMaintenance user is not added to the Administrators group
Issue
PME maintenance tasks fail with error 0x1F4 if IONMaintenance user is not added to the Administrators group

In the  SQL Error logs, you may see the following error
"Login failed for user 'ServerName\IONMaintenance'. Reason: Failed to open the explicitly specified database 'ION_Network'. [CLIENT: <local machine>]"

Error message

Facts
  • If IONMaintenance user is added to windows administrator group, the tasks run successfully
  • IONMaintenance user roles are correctly set up in SQL for the 4 PME databases
  • IONMaintenance user has full write access to the  Backup destination folder
  • IONMaintenance is a member of "Users" group


Product Line
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
PME Standalone systems

Cause
The privileges granted to the group BUILTIN\Users has higher priority over User privileges.

Resolution
In SQL, grant "db_backupoperator", "db_ddladmin" and "Maintenance" Membership for "BUILTIN\Users" for all PME databases


ION Maintenance Privileges

User permissions


Schneider Electric Global

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: