Issue
How to obtain all the details of all SQL Jobs created on a SQL server instance.
Product Line
ION Enterprise 6.0. x
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Environment
SQL Server 2005, SQL Server 2008 R2, SQL Server 2012, SQL Server 2014, SQL Server 2016, SQL Server 2017
Cause
For daily monitoring purposes or for troubleshooting SQL job issues, obtaining information about the SQL jobs via a single query can be very useful and time saving alternative method.
Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
This query will provide the sql server job details for all jobs present. It will provide job name, job status, Last run date of job & job execution status (failed or successful)
It may also be modified to add or change the fields reported as per requirement.
To obtain these job details, log into SQL Server Management Studio and run the attached SQL script (SQL_Job_Details.sql).
Alternatively, execute the query(s) below:
Use msdb
go
select distinct j.Name as "Job Name", --j.job_id,
case j.enabled
when 1 then 'Enable'
when 0 then 'Disable'
end as "Job Status", jh.run_date as [Last_Run_Date(YY-MM-DD)] ,
case jh.run_status
when 0 then 'Failed'
when 1 then 'Successful'
when 2 then 'Retry'
when 3 then 'Cancelled'
when 4 then 'In Progress'
end as Job_Execution_Status
from sysJobHistory jh, sysJobs j
where j.job_id = jh.job_id and jh.run_date =
(select max(hi.run_date) from sysJobHistory hi where jh.job_id = hi.job_id ) -- to get latest date
Released for:Schneider Electric Global