When using preset speeds and an analog speed input which one takes priority?
When the inputs for the preset speeds are high they override the analog speed. If the preset speed inputs are low then the drive will run at the analog speed input speed or LSP if no signal is present.
CTA-ID : 2001374
Released for:Schneider Electric Global
Explore more
Range:
Altivar Process ATV900
Altivar Process ATV600
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.