As shown in the picture below, the DWORD_TO_REAL function doesn't allow to convert a DWORD variable as a real value with a floating point based on the IEEE-754 standard.
In order to convert a DWORD variable to a real value following the IEEE-754 standard, we have to create a DUT - UNION type.
DUT definition:
Released for:Schneider Electric Global