Issue:
Monitor the DC bus current with a DC bus tie on the ATV930 series drive.
Product Line:
Altivar ATV930 series only
Environment:
All
Cause:
Wants to read the dc amps when two drives are connected via DC bus.
Resolution:
You can't view the DC bus amps on the HMI so you would need to use a DC amp clamp on accessory for your meter.
Released for:Schneider Electric Global