Issue:
Ambient heatsink temperature when the THD is 100 percent?
Product Line:
ATV630 Drive
Environment:
All
Cause:
Heatsink temperature if the thd (Drives thermal temp) reads 100 %.
Resolution:
If the THD is reading 100% this is around approximately 85 degrees C.
The drive will trip on OHF at 118% or approximately 100 degrees C or between 90 degrees C to 105 degrees C.
Released for:Schneider Electric Global