{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Setup the ATV340 Drives Ethernet IP address using the optional remote keypad display.

Issue:

ATV340 programming setting up the Ethernet IP address using optional HMI.

Product Line:

ATV340 with optional keypad VW3A1113 or VW3A1111.

Environment:

All

Cause:

Programming setup Ethernet IP address

Resolution:

This programming example is if you use one of the optional keypad to program your drive.

[Communication] -[Comm parameters]- [Embd Eth Config]

-[Embd Eth Config] EtE- Menu

PAn= Add a Device name

iNOO= IP mode set to NAnu or Fixed

iCO= IP Address (IC01, IC02, IC03, IC04).

iNO= Subnet mask (IM01, IM02, IM03, IM04).

iGO= Gateway address (IG01, IG02, IG03, IG04).

After setting up your IP address and subnet address etc you will need to power cycle the drive.