Issue:
Use the VW3A1113 HMI to complete ATV340 firmware update.
Product Line:
VW3A1113
Environment:
All
Cause:
HMI is used to finalized the firmware update and its missing menu 7.3.
Resolution:
No you can not use the VW3A1113 HMI to complete the firmware update on the ATV340 version Drive. The VW3A1113 HMI will not display menu 7.3 which is needed to finalize the firmware update. You have to use the VW3A1111 to complete the firmware update.
Use the VW3A1113 HMI to complete ATV340 firmware update.
Product Line:
VW3A1113
Environment:
All
Cause:
HMI is used to finalized the firmware update and its missing menu 7.3.
Resolution:
No you can not use the VW3A1113 HMI to complete the firmware update on the ATV340 version Drive. The VW3A1113 HMI will not display menu 7.3 which is needed to finalize the firmware update. You have to use the VW3A1111 to complete the firmware update.
Released for:Schneider Electric Global