Issue:
ATV630 and ATV930 drive for sourcing or sinking mode?
Product Line:
ATV630 and ATV930 Family
Environment:
All
Cause:
Setting up the logic inputs to switch on with a sinking input to com.
Resolution:
The sink source switch is located on the face of the drive under the terminal IO block. Sink position is on the left and source position is on the right.
Released for:Schneider Electric Global