Issue:
LCR address 3204 motor current units or values for the ATV340 Drives.
Product Line:
ATV340 Drives.
Environment:
All
Cause:
Motor amps are reading to high over Ethernet or address 3204 LCr.
Resolution:
The unit of LCR are
From ATV340 0.75kw to ATV340 15kw, the unit is 0.01A.
From ATV340 18.5kw to ATV340 75kw, the unit is 0.1A .
Released for:Schneider Electric Global