{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Will the ATV630 BACnet option card VW3A3725 support BACnet IP?

Issue:

Will the ATV630 BACnet option card VW3A3725 support BACnet IP?

Product Line:

ATV600 with VW3A3725 option card.

Environment:

All

Cause:

Offer selection for BACnet IP

Resolution:

The VW3A3725 option card is fieldbus BACnet MS/TP only and is not BACnet IP compatible.