{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why does the connection status LED stay gray when updating the ATV930 or ATV630 Drives firmware using the EADM software tool?

Issue:

What do the status LED colors mean when updating the Process Drives firmware using the EADM software tool?

Product Line:

EADM tool with ATV630, ATV930 or ATV340

Environment:

All

Cause:

Status indicator LED meaning

Resolution:

There are three colors for the status:

-    Green – Drive reachable and logged-in

-    Yellow – Drive reachable and not logged-in

-    Gray – Drive not reachable (drive power off / disconnected)

EADM file 1

EADM file 2