{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you run a small test motor with the ATS480 soft start?

Issue:
How do you run a small test motor with a ATS480 soft start?

Product Line:
ATS480

Environment:
Small test motor

Cause:
n/a

Resolution:
Go to Menu 3.3: Set [Small Motor Test] SST to YES. The PHP (Phase Loss Monit) will be forced to NO and Control Mode (CLP) is forced to Voltage Control (VC).
To start the test, apply a Run command to the soft starter by pressing the RUN button on the display terminal or via the STOP and RUN control terminals.
To stop the test, apply a Stop command to the soft starter by pressing the STOP / RESET button on the display terminal or via the STOP and RUN control terminals.

Note:
The [Small Motor Test] SST test function is set to [No] when the soft starter control supply is disconnected.
Upon next power-up the soft starter, including [Phase Loss Monit] PHP and [Control Mode] CLP, will return to its previous configuration.