Issue:
Changed both HMI baud rate and fieldbus baud rates to 9600 and now HMI is not working how can you reset it?
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
HMI baud rate needs to be set to 19.2 in order for the HMI to work.
Resolution:
If you have changed both HMI and fieldbus baud rates and the HMI is not connecting, you will need to order the
TCSMCNAM3M002P cable from the supplier to be able to connect to Somove and go in and reset the HMI baud rate back to 19.2K.
or if you have the Ethernet password you can connect via Ethernet to Somove and go in and change the HMI baud rate back to 19.2K.
Released for:Schneider Electric Global