{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you read or access RSTP data over Ethernet on the ATV600 or ATV900 Process drives?

Issue:

Reading RSTP data over Ethernet on the ATV 600 and ATV900 Process drives.

Product Line:

ATV600 with VW3A3720 option card or ATV930 Drives.

Environment:

All

Cause:

Reading RSTP over serial communications.

Resolution:

ATV900 or ATV600 with Ethernet IP card are compatible with other RSTP devices (switch, PLC).

However, there is no way to read the RSTP status over the Ethernet network.