Issue:
What does the Z suffix mean on the ATV630 and ATV930 Drives?
Product Line:
ATV630 and ATV930 Drives.
Environment:
The IP20 only
Cause:
Cabinet Integration versions of the ATV630...Z and ATV930...Z drives.
Resolution:
The Z suffix on the ATV630....Z and ATV930....Z are the cabinet Integration version Drives and will ship without the
-No conduit kit (size 1-5)
-No top cover
-No keypad or HMI
The drive will be IP20 rated.
Best Regards,
Gary Richardson
Released for:Schneider Electric Global