{}

Can I simulate PTO function blocks in SoMachine Basic?

Issue: Can I simulate PTO function blocks in SoMachine Basic? Product Line: M221, TM221 Resolution: Just like the PID blocks, you cannot simulate PTO functions blocks in SoMachine Basic. You will...

A 415V motor, class F insulation with dv/dt capability of 1 KV/μS, Can can...

Generally the motor with Class F insulation is considered as VFD graded motor, but it is specified that the dV/dT withstand capacity is 1 KV/μS. Hence we can not consider this motor as VFD graded...

How to read swapped floating point values in Modbus

Issue The user has a Modbus device containing swapped floating point registers and wants to confirm the values being read by software such as Power Monitoring Expert (PME), with SwappedFloat...

What can cause an OPF2 fault on the ATV12 drives?

Issue: OPF2 on the ATV12 drives? Product Line: Altivar ATV12 Environment: All Cause: Drive is trying to run the motor but is tripping on an OPF2 fault. Resolution: OPF2 fault means 3 output phase...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our Generic Knowledge FAQsGeneral Knowledge

Insulation Resistance Testing and Humidity

Issue: How does humidity affect insulation resistance testing results? Product Line: Circuit Breakers Environment: Molded case and insulated case breakers Resolution: High humidity can drastically...

What’s AC-3e rating means and what’s their application ?

AC-3e rating is the capability of the contactor for starting and switching off high efficiency squirrel cage asynchronous (IE-3/ IE-4) motors during running and reversing operations, which have...

Symmetra PX 250/500K power module life cycle alarm

Issue: Symmetra PX 250/500K power module life cycle alarm Product line: Symmetra PX 250/500K Cause: Customers may call in to request an FSR or ask how to reset the life cycle alarm on the power...

How to establish the communication with S7-1500 PLC if using TIA Portal...

In PLC side: 1.Use TIA Portal V11-V16 to configure the PLC communication settings. 2.Select the PLC and enter the correct version of the firmware (We can check for the firmware version of the PLC in...