Search FAQs
Whether Withdrawable or Fixed NSX MCCB can be installed in Horizontal Position ?
The Compact NSX circuit breakers may be installed horizontally, vertically or flat on their back, without derating performance levels.
There are three installation versions:
1. Fixed
2. Plug-in (on a base)
3. With draw-able (on a chassis).
For the Plug-in and Withdrawable versions the components must be added (base,chassis) to the fixed version.
For details pl refer the attachment.
There are three installation versions:
1. Fixed
2. Plug-in (on a base)
3. With draw-able (on a chassis).
For the Plug-in and Withdrawable versions the components must be added (base,chassis) to the fixed version.
For details pl refer the attachment.
Released for:Schneider Electric Global
Attachment(s)
Explore more
Range:
Explore more
Range: