The ProWORX 32 Full and Lite packages have the same functionality. There are no differences/limitations between the two packages other than the PLC s they support.
372SPU78001PDEV.....ProWORX 32 Full Offline/Online Client Package (supports all of the Momentum, Quantum, 984 Series Slot Mount, Compact, Modicon Micro 110CPU, Modicon Micro984, 984A,B,X Chassis Mount, Atrium and VME controllers).
372SPU71001PLDV.....ProWORX 32 Lite Offline/Online Client Package (only supports all of the Momentum, Compact and Modicon Micro 110CPU controllers).
Released for:Schneider Electric Global