Goals and Symptoms
Procedure for adding an IP address onto a ProworX32 project for a Momentum 171CCC9x0 x0 M1E processor.
Causes and Fixes
· Start up ProworX32
· Open your project
· Select Configuration
· Enter a value into the Config Extension Size (ex. 200)
· This value can be modified later depending on the Config Extension Used value
· Select Configuration Extensions
· Check and highlight TCP/IP
· Enter New IP and Subnet Mask info
· Save project
· Select Communications
· Select which form of connection you currently have to download your project.(Modbus, Modbus Plus or TCP/IP)
· Or enter the PRODUCTS current IP address that is stored on the processor if your just changing to a new IP address.
· Save project
· Open Controller tab
· Select Write All
· Select Write
· Make sure you get the Write to M1 960-20 Complete in the Message Central window
· Select Communications
· Enter New IP address info
· Open Controller tab
· Select Transfer to Flash/EEPROM…
· Select Transfer
· Recycle power to your Momentum processor to make sure all changes were saved
· Select Start/Stop…
· Check your logic and make sure all is fine
Released for:Schneider Electric Global