Issue
Is it possible to perform a Cold Reset in a logic subroutine using a SoMachine V4.3 / EcoStruxure Machine Expert Logic controller?
Product Lines
Modicon M238, M258, M241, M251, M262, HMISCU
SoMachine v4.3, EcoStruxure Machine Expert
Environment
PLC Programming software in Windows
Resolution
The two steps required are:
1. Set/write PLC_W.q_wPLCControl := PLC_W_RESET_COLD
2. Write PLC_W.uiOpenPLCControl := 6699
For example, the Structured Text (ST) code would look like this:
IF PLCColdReset=TRUE
THEN
PLC_W.q_wPLCControl:=4;
PLC_W.q_uiOpenPLCControl:=6699;
END_IF
For more information, search for the "PLCSystem Library Guide" for the specific PLC family in the Software Help system or the User Guide PDF on our website.
Is it possible to perform a Cold Reset in a logic subroutine using a SoMachine V4.3 / EcoStruxure Machine Expert Logic controller?
Product Lines
Modicon M238, M258, M241, M251, M262, HMISCU
SoMachine v4.3, EcoStruxure Machine Expert
Environment
PLC Programming software in Windows
Resolution
The two steps required are:
1. Set/write PLC_W.q_wPLCControl := PLC_W_RESET_COLD
2. Write PLC_W.uiOpenPLCControl := 6699
For example, the Structured Text (ST) code would look like this:
IF PLCColdReset=TRUE
THEN
PLC_W.q_wPLCControl:=4;
PLC_W.q_uiOpenPLCControl:=6699;
END_IF
For more information, search for the "PLCSystem Library Guide" for the specific PLC family in the Software Help system or the User Guide PDF on our website.
Released for:Schneider Electric Global