{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the difference between TIME and LTIME data types in Machine Expert?
TIME is a 32 bit data type. The resolution is in milliseconds.

LTIME is a 64 bit data type. The resolution in nanoseconds.


Example of variable declarations:

var_0 AT %MD0: TIME;    // %MD0 overlaps with %MW0 and %MW1
var_1 AT %MD1: TIME;    // %MD1 overlaps with %MW2 and %MW3

var_2 AT %ML0: LTIME;   // %ML0 overlaps with %MW0, %MW1, %MW2 and %MW3
var_3 AT %ML1: LTIME;   // %ML1 overlaps with %MW4, %MW5, %MW6 and %MW7



Schneider Electric Global