{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the TM251MESE support simultaneous use of both EtherNET/IP and ModbusTCP master?
Issue:
Is it possible to use both Ethernet/IP and Modbus TCP/IP at the same time on an TM251MESE?

Product Line:
PLC, M251

Environment:
SoMachine

Cause:

Resolution:
Yes, it is possible to have a mixed network of EtherNet/IP adapters and Modbus/TCP servers but it will be limited to 16 devices in total. The scanner resources tab can be used to check the performance of the network.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global