Connect and change parameters on a LXM32 drive using SoMachine
Published date:
29 March 2019
Issue:
Can I connect and change parameters on LXM32 servo drive using SoMachine?
Product Line:
SoMachine
Resolution:
In SoMachine, when you add a LXM32 drive to the network, you can double click it and go to the 'Configuration of the device' tab, where you can see a SoMove-like screen (See attached).
Just like the SoMove interface, you can connect to the drive and upload/download/edit parameters.