{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the server/client side requirement of Citect Anywhere?
Server-side requirements:-

• Windows Server OS
• Microsoft Remote Desktop Services (RDS) CALs
• Vijeo Citect / CitectSCADA v7.20 (SP5) and above
• Citect Control/View Only Client licenses
• Citect Anywhere licenses

Client-side requirements:-

Any operating system with the HTML5-capable browser
  • Internet Explorer® 10 or higher
  • Safari® 8 or higher
  • Chrome™ 33 or higher
  • Microsoft® Edge